Installation Instruction

1. Create a file folder and name it C:\ProPVplus
2. Unzip all files to this folder
3. Double-click on file SETUP.EXE

The software installs itself and is ready to be used.

Standard Parameters for each pump size are pre-programmed
on each module. The PAR-files attached here are available
as back-up.

The Calculation Tool is available if a fine tuning is
needed.


Note: 	Cable PQDXXA-KABEL is needed to connect the
	digital module to the PC.